Overview
========

The lwip_udpecho demo application demonstrates a UDP echo demo on the lwIP TCP/IP stack with bare metal KSDK or
FreeRTOS, which uses the UDP protocol and acts as an echo server. The application sends back the received UDP packets
from the PC, which can be used to test whether a UDP connection is available.


Toolchain supported
===================
- IAR embedded Workbench  9.10.2
- Keil MDK  5.34
- GCC ARM Embedded  10.2.1
- MCUXpresso  11.4.0

Hardware requirements
=====================
- Mini/micro USB cable
- Network cable RJ45 standard
- MIMXRT1170-EVK board
- Personal Computer

Board settings
==============
This example uses 1G port(J4) as default. If want to test 100M port(J3), please define the global macro EXAMPLE_USE_100M_ENET_PORT.

Prepare the Demo
================
1.  Connect a USB cable between the PC host and the OpenSDA(or USB to Serial) USB port on the target board.
2.  Open a serial terminal on PC for OpenSDA serial(or USB to Serial) device with these settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Insert the Ethernet Cable into the target board's RJ45 port and connect it to your PC network adapter.
4.  Configure the host PC IP address to 192.168.0.100.
5.  Download the program to the target board.
7.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo
================
1. When the demo runs, the log would be seen on the terminal like:
		Initializing PHY...

		************************************************
		 UDP Echo example
		************************************************
		 IPv4 Address     : 192.168.0.102
		 IPv4 Subnet mask : 255.255.255.0
		 IPv4 Gateway     : 192.168.0.100
		************************************************
2. From the command window, type echotool 192.168.0.102 /p udp /r 7 /d hello
	NOTE: The echotool.exe application can be found here https://github.com/PavelBansky/EchoTool
3. The command window should get response:
		Hostname 192.168.0.102 resolved as 192.168.0.102

		Reply from 192.168.0.102:7, time 1 ms OK
		Reply from 192.168.0.102:7, time 1 ms OK
		Reply from 192.168.0.102:7, time 0 ms OK
		Reply from 192.168.0.102:7, time 0 ms OK
		Reply from 192.168.0.102:7, time 0 ms OK

		Statistics: Received=5, Corrupted=0